Other Parts Discussed in Thread: AMC1305M25, AMC1304M25, ADS1118, ADS1248, TMS320F28377D, ADS5560, ADS1610, ADS5562, AMC1210
HI,
I'm interested in the AMC1305M25 ADC chip, I'm hoping to achieve 16bit resolution at 20 MSps data conversion using this chip with an MCU (not really dependant on the MCU, but I'm hoping to use a MCU if I can).
The analog signal I'm hoping to capture will have a highest frequency component around 400 KHz, so I wanted an ADC that can do faster than 10 MSps at 16 bits.
But looking at the spec sheet of AMC1304M25, all the characteristic curves which has input frequency for the x axis only goes up to 100 kHz.
This seems to me like a low cut off for something that is sampling at 20 MHz. Can anybody give me some clarity to my logic, or point out what am I missing here?
Thank you in advance.
Oliver