I intend to measure two 4-wire PT100 RTD's on a single ADS1248. Please advise on the best connection method to do this. I will refer to the four RTD wires as 1+, 2+, 3-, 4-. My intention was to connect as follows:
RTDA_1+ connected to IEXC1
RTDA_2+ connected to AIN0
RTDA_3- connected to AIN1
RTDA_4- connected to REFP0 through 1.65k resistor.
RTDB_1+ connected to IEXC2
RTDB_2+ connected to AIN2
RTDB_3- connected to AIN3
RTDB_4- connected to REFN0 through 1.65k resistor.
The advantages to this option I believe are using the dedicated IEXC sources, which doesn't require waiting for the IDAC to settle as I switch between the two measurements... which would be the case if I used the AINx pins for excitation. I expect to sample at 160SPS. AVDD is 3.3V.
Is there any advantage/disadvantage to using a shared reference connection (both connected to REFP)? Any advantage/disadvantage for using the IEXC versus AINx for excitation?
Thank you.