Hi,I'm developing a reflective pulse/oxy device detect heartrate by toe,using AFE4400,I find that someone is very difficult to get the PPG signal,we have the same product using transmissive type,and it works well。The reflective type is too difficult because the signal is weak and easy operational when adjust the amplifier ,either adjust the LEDCNTRL or TIAGAIN,the result is not very good,it puzzled me a long time.So i want to know someone‘s advice who has faced with much the same problem.How can i improve the signal,to amplify it to fit the arithmetic?Shall I select other reflective pulse/oxy sensor or adjust the register of AFE44xx?thanks very much!
1. good(RED、IRed 、weight)
2.Bad signal(RED、HR)