This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1274 CLK duty spec

Is there duty spec for FCLK in term, are they sensitive to variation of duty?,

Can it work say 10% duty

Thanks.

  • Dear Richard,

    our application engineers responsible for this device are already on vacation. It might probably take one week till we can definitely confirm if duty-cycles as low as 10% are possible.
    According to the datasheet (timing parameter t_CPW, p.8 in the datasheet) the duty cycle in SPI mode could be as low as 0.15% when running at the slowest f_CLK rate of 100kHz. But I don't believe this is really possible. At the highest f_CLK frequency of 27MHz the duty cycle is limited to 40%.

    Jitter on the clock signal will have a negative effect if you try to measure AC signals. The higher the frequency of the signal the larger the effect will be.

    Regards,