Hello,
| Mean (V) | Vrms | Vpp | Mean (I) | Irms | Ipp | |
| LED 2 (RED) | 4.04E-02 | 2.52E-03 | 1.21E-02 | 1.14E-08 | 7.13E-10 | 3.42E-09 |
| LED 2 (RED) AMBIENT | -5.79E-03 | 2.21E-03 | 6.91E-03 | -1.64E-09 | 6.25E-10 | 1.95E-09 |
| LED 1 (IR) | 5.18E-02 | 3.46E-03 | 1.80E-02 | 1.47E-08 | 9.79E-10 | 5.08E-09 |
| LED 1 (IR) AMBIENT | -5.61E-03 | 2.24E-03 | 7.18E-03 | -1.59E-09 | 6.32E-10 | 2.03E-09 |
| LED 2 (RED) - LED 2 (RED) AMBIENT | 4.62E-02 | 1.27E-03 | 6.54E-03 | 1.31E-08 | 3.60E-10 | 1.85E-09 |
| LED 1 (IR) - LED 1 (IR) AMBIENT | 5.74E-02 | 2.68E-03 | 1.37E-02 | 1.62E-08 | 7.58E-10 | 3.88E-09 |
If there is no baseline drift in the signal, R=(6.54E-03/4.62E-02)/(1.37E-02/5.74E-02 )? Is it right?