Hi,
I just received the ADC1xDxxxx(RF)RB Gigasample Reference Board. It says "Copyright 2013" and "PCB REV B." I have the 1.6 GSPS ADC.
I've downloaded the support packages that has schematics and the Xilinx project and .bit file. But the names on the schematic do not seem to match up with the names silkscreened onto the board. Some of the speed settings in the Xilinx project (.ucf file, DCM modules) do not appear to match the 1.6 GSPS device. Going down the directory tree, the titles change between different speeds.
So, I would like to make sure that I have the correct schematic and Xilinx FPGA files, to eliminate any confusion. The board powered up OK and runs with the software. I did not receive a CD with the board, I wrote in earlier, I downloaded another set of files which also do not appear to match, so I thought I'd stop and ask for help.
Thanks,
Rich Katz