Hi
My customer is using ADS1248 .
Could you let me know the termination of unused AIN6,7-pin?
Which of the AVDD connection or the AVSS connection or the open is best?
Thanks
Shimizu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
My customer is using ADS1248 .
Could you let me know the termination of unused AIN6,7-pin?
Which of the AVDD connection or the AVSS connection or the open is best?
Thanks
Shimizu
Shimizu-san,
The connection of unused analog input pins can slightly impact the leakage currents of the other channels. For the lowest leakage on the used pins, we recommend leaving the unused pins floating. If customers don't want to leave inputs unconnected, the next best option is to connect them to AVDD. ,If there is a risk of ESD or EMI pickup for an unconnected analog inputs, then the inputs can be tied to AVDD through a pullup resistor.
Joseph Wu