Other Parts Discussed in Thread: ADS5409, ADS5402EVM
hello,
in the datasheet on the ADS5409 no recommendation on connection scheme of the input signal.
I use a scheme with double the transformers, the band of the input signal 70 - 270 MHz, AC - сupling.
The question is,
In ADS5402EVM board, there is an option to bias the common mode level of the analog signal. In which case this option is required?
In my application signal is always AC - сupling. I can not bias input signal to VCM?
The second question,
100 ohm termination resistor. I can not put it? In which case it is needed?