This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12J4000 pll_locked status issue

Hi,

On our own board, we use several ADC12J4000 connected to a FPGA.

We are able to synchronize the JESD204 links and make acquisitions without problem at 4GHz.

However the PLL_LOCKED status bit (reg 0x205 : JESD_STATUS) is always stuck to '0' for all the ADCs. 

The quality of the clock in input of the ADC is very good with a differential input level of 0.8Vpp.

We tested various clock frequency between 1.5GHz and 4GHz, PLL_LOCKED bit is always down.

Do we have to worry about this status while everything is working properly?

Any idea of what could cause this issue?

Kind regards

Florian