This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4403/AFE4490 Minimum connections to MSP

Other Parts Discussed in Thread: AFE4490

All:

From the TODA-00311 "Miniaturized Pulse Oximeter Reference Design," it appears that the minimum connections needed between the microcontroller and AFE device are the following:

SPI connections:

SPISTE

SPISIMO

SPISOMI

SCLK

 

Additional I/O:

AFE_PDN

ADC_RDY

RESET

DIAG_END

 

What is the minimum set of connections required?

4 SPI for sure + RESET

Can the other 3 I/O be handled via commands?

It looks like AFE_PDN may be a required I/O for power down.

It looks like ADC_RDY is not available as (status) register value, thus it also is required. Would it make sense to be able to poll for ADC_RDY if it were available, thus saving an I/O?

Also, it looks like DIAG_END is not available as (status) register value, thus it is also required. Again, would  it make sense to be able to poll for DIAG_END if it were available, thus saving an I/O?

On the AFE4490, there are two additional I/Os - LED_ALM and PD_ALM. It looks like these are also available as (status) register values, so in an application that would use the AFE4490, would it be necessary to also include these as I/O's to the microcontroller?