Hello,
I was wondering whether ADS8556/7/8 could use a non symetric high voltage supply. I need to simultaneously sample voltage between 0 and 5V (maybe 12V) with 16 bits resolution and 500kSps, and to reduce system cost and complexity, was considering to only use a single 5V/GND (or a double +5V/+12V/GND in the second case) supply for analog and high voltage supplies.
I could not find any statement whether this configuration is supported or not in the datasheet.
Thanks
François