In regard to ADS1274 D-FlipFlop, SCLK discussion. I wish to establish if the circuit really need latch for SM320F28335?
Below is the connection configuration
ADS1274 SM320F28335 (McBSP)
SCLK(28) MCLKRA (This is FMOD source for ADS1274)
CLK(27) -> MCLKRA (SCLK and CLK tied together)
FSYNC(29) -> MFSXA
TDM(20) -> MDRA
MDXA = NC
MFSRA = NC
MCLKXA connect to external clock
Configure for TDM, FSYNC, LOW POWER or HIGH RESOLUTION (VIA jumper resistor).
I have 3KHz with 12KSPS or 24KSPS (configure FMOD clock close to 3MHz or 6MHz from MCLKRA)
Do I need latch?, can you shown me if this violate timing or not.
On seperate topic.......I have CH1 and CH2 only (CH3 and CH4 disabled), should I use fixed data or dynamic so I do not need to accept CH3 and C4.