This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Conflicting datasheet specs for DAC8814 Clock Input Frequency and Clock Width High/Low

Other Parts Discussed in Thread: DAC8814

We're using a DAC8814 in our application.  However, the datasheet appears to provide conflicting specifications for the DAC8814 Clock Input Frequency (fclk) and Clock Width High/Low (tch/tcl).

  • Fclk = 50MHz min
  • tch/tcl = 10ns min

The only frequency where the above are satisfied is exactly 50MHz.  It appears to me that one of the above needs to be defined as a maximum.  Should the datasheet be revised to state the following?

  • Fclk = 50MHz max
  • tch/tcl = 10ns min

Thanks,

--Todd W