Hello Support,
I have some questions regarding the ADS1248 in order to double check my design before I get something built.
I have to measure 6 single-ended inputs (referenced to GND) having an amplitude ranging from 0V (GND) to 2V. Each of the 6 single-ended inputs is connected to a AINx pin (x=0-5) and AIN6 is connected to GND for reference.
In my setup: I have DVDD = 3.3V and AVDD = 3.3V. I have VREFOUT and VREFCOM connected to a 47uF ceramic capacitor and VREFCOM to GND; I use internal Vref (=2.048V). I would like to set PGA=1 in my application.
I have tied DGND,CLK and AVSS to GND.
I would like to know if this setup (connections and PGA settings) is OK and what I can do in order to optimize it.
If I want to add a thermocouple input in my design, do I need an additional ADS124x component? Or can I connect it to AIN7 (using suitable conditioning circuits)?
Thank you in advance.
Kind Regards
Gaetano