This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Use of uPP port of C6746 for A/D converter

Other Parts Discussed in Thread: ADC14L020

There is a list of compatible TI A/D converters, but this list is not exhaustive. 

We are thinking of using the ADC14L020 placed on the uPP port.  I do not see anything incompatible but wanted to ask if perhaps some problem is lurking there that I have not seen.  From the point of view of speed, timing, voltage levels, it looks OK.

The other question is about evaluation tools.  Looking at the schematics for the OMAP138 or C6748 EVM, the uPP is not brought out to an interface connector.  Is there any other evaluation tool that would allow using the uPP?  After all, I understand that the main difference between the 6747 and the 6748 is that the 6748 has the uPP.  I would hope that there is an EVM to allow checking this out?