This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Remote patient Monitoring System

I am a student in YSU and I want to build a prototype of remote patient  monitoring system so I need wireless ECG sensor which can be embedded in textile or just wearable ECG sensor with Bluetooth. Also I need micro controller ( MSP430x22x2 or MSP430x22x4)  with Bluetooth and all  other requirements such as Amplifier, Filtering, etc.. the micro controller will receive the signals from the ECG sensors by Bluetooth then send them to smartphone . I need Lithium- Ion Battery either rechargeable or nonchargeable  to provide the micro controller  and sensors with required power. finally, I need wires to transfer the power from the battery to sensors and micro controller.

Ali Naeemah