This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC3484EVM plugged into TSW1400EVM

Hi,

I have purchased a DAC3484EVM plugged into TSW1400EVM in order to generate arbitrary analog pulses the I need for my laser external intensity modulator. I installed all the software including DAC3484x_GUI_v3p8.vi and High Seed Data Converter Pro v3.0

Everythings looks OK my laptop detects the board and after  loading all the green LEDs of FGPGA board lights green with no problem. I also follow the instructions on USER's Guide DAC348xEVM pages 4 through 9 with no problem. Then, as a first test I load of the files in the test folder called "single_tone_complex_32768_250MSP_BW_25.1MHz.csv". I see that the file gets loaded and its fft shown on the screen. However, when I send the file I can not detect the signal on the scope on any of the four channels?? I selected channel #1 initially but I tried all the other channels?

What is wrong with my setup?

I tried different configuration files but none of them worked? I can not see any signal on the scope??

I have connected a 800 MHz clock input of the board??