Other Parts Discussed in Thread: ADS42LB69, ADS42LB49EVM
Hello,
Our customer is confirming the time to valid data of ADS42LB69 by EVMs.
Then the capture data is intermittent.
I found the time to valid information from the following post.
http://e2e.ti.com/support/data_converters/high_speed_data_converters/f/68/t/376025
Q1: Is the first capture data at the 1st clock data or 15th clock ( 14clk cycle) data ?
Q2: Does the capture board(TSW1400) operate correctly when ADC got the clock input at the limited time period after the capture starting?
<test sequence>
1. Power supplies to ADS42LB49EVM and TSW1400.
2.Input the 1MHz Sinwave of SG to ADC input.
3.ADC capture started (250MHz, 65536 points data captured)
4.Input the 250MHz Clock during any period.
5.Capture finished
CLK input is DC coupling, LVPECL input. Vcm is 2V, Amplitude is 1Vpp diff)
Best Regards,
Ryuji Asaka