Hi there,
I am developing an AFE4490 circuit with the red and IR LED (Marubeni SMT735-890) in a common anode mode. The AFE4490 is mainly powered from 3.0V (regulated), while the TX section is directly from a LiPo battery (3.7V, unregulated).
There are a few ambiguities that I need clarified, which has yet been answered in post http://e2e.ti.com/support/applications/high_reliability/f/30/t/383235. The nearest answer was in http://e2e.ti.com/support/applications/high_reliability/f/30/p/393157/1388344 , but it was for the AFE4403.
Clause 1) Figure 67 of the AFE4490 datasheet shows the anode of the LED connected to "External Supply" and LED_DRV_SUP left unconnected.
Clause 2) Figure 132 shows the anode of the LED connected to LED_DRV_SUP. Is this LED_DRV_SUP the same as that in Clause 2?
Clause 3) The table in Section 7.3 shows that LED_DRV_SUP and TX_CTRL_SUP must be within +-0.3V of each other. Must they be connected?
Does it mean that:
* Clause 1 is incorrect (LED_DRV_SUP must be connected)?
* LED_DRV_SUP has to be connected to "External Supply" (Clause 2)?
* TX_CTRL_SUP has to be connected to LED_DRV_SUP (Clause 3)?
Hope to hear from you soon.
Best regards,
Royan