Hi. I have DAC3484EVM plugged into TSW1400. My goal is to create two pulse waveforms with amplitude of 2Volts at 1700 Hz with pulse duration of 2 us.
The pulse is on for 2 us then off by 588 us.
Channel #1 and Channel #2 needs to be delayed from each other by 100 us. Also, I would like to use onboard clock (CDCE62005)?
Q1-What file do I need to load for utilization of on board clock??
Q2- Is there any example of a file for creating a pulse waveform at any lower frequency (1KHz or 10 kHz)?
Q3- I see that many people who are using DAC3484 board are using it for creating tones at much higher frequency than 1700 Hz?
Q4-Is there any limitations to what I am trying to do with this hardware?
I appreciate your input.
Thanks
Joseph