Hello,
ADS1192 internal clock accuracy is 0.5%,typ and 1.5%,max, and AFE4403's Murata ceramic resonator is 0.5%,typ. However, to pass regulations like FDA, the clock accuracy is beter to be less than 0.1% or better less than 100pm, so can you suggest solutions to implement higher accurate clocks?
Thanks.
Ming