Hello Praveen,
Here is the connection for AFE4403 as Figure 52 and 53 of the spec:
-
3 LEDs are in common anode configuration.
-
The 3 LEDs’ anodes connect to 5.0V.
-
Both LED_DRV_SUP and TX_CTRL_SUP connect to 3.0V
However, there is an huge leakage current of more than 15mA from TXP/TXN to LED_DRV_SUP/TX_CTRL_SUP (3.0V) and force the 3.0V to be higher. After cutting off the PCB traces of TXP/TXN, the leakage is gone. The date code of the AFE4403 is 48AXZDI.
In this formal project, we have met this leakage issue, but in our evaluation board, the connection (except LED_DRV_SUP and TX_CTRL_SUP to 3.3V) is no problem. Please comment.
Thanks.
Ming