Other Parts Discussed in Thread: ADCPRO
Hello,
I am trying to start up an ADS1282EVM-PDK and have problems.
- Latest ADCPRO, 2.0.1Build 4
- Latest drivers, downloaded from TI toady
- Provided 6V external power supply connected
- EVM: ADS1282EVM 2.0.0.0
When I start up the software I see these status messages:
- Reading Binary file
- Downloading binary file
- USB connection established
- Download successful
- DSP not ready...retrying
- Popup "The firmware load has failed due to connection timeout..."
- EVM/HW incompatible
I only have the 6V supply connected. Are any of the other supplies required to start up the board or is this a DSP error?
The main board has BOM revision D. The J13 jumpers do not look exactly like in the manual and there is no S4 USB / ROM switch.
It says in the manual "Set jumper J4 low to indicate that the EVM board is an ADS1282EVM." but I guess this is S4, not J4 as J4 is the connector to the sub-board.
I would appreciate any help I can get on this.
Am I doing something wrong or is the board fried?
Thanks in advance.