This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300 calibration steps to perform the impedance measurement

Other Parts Discussed in Thread: AFE4300

Hello!

I have questions regarding the slope and offset calculating in FWR and IQ mode. The explanation and example in Section 2 is ambiguous.


If I want to use FWR mode for 3 different frequencies like 5 kHz, 50 kHz and 100 kHz, so should I measure the resistance of reference resistors only onetime unter 64 kHz and ADC 64 SPS?
What is the frequency and settings for measure of I and Q voltage of the reference resistors Rx and Ry in the Step 2 Section 2.2?  If I want to use IQ mode for frequencies like 8 kHz and 16 kHz..
In the Step 3 do I calculate slope and offset, is equation for slope_IQ = (Ry - Rx) / (Mag_Ry – Mag_Rx)  and offset_IQ = Rx – slope_IQ x Mag_Rx ? Where can I find the equation for slope and offset?

In the example for IQ you use the slope value from FWR mode measurement, is it correct?

Thanks

Æ