Other Parts Discussed in Thread: ADS131E08, MSP430F2619
Hi TI Team,
We are in the process of development of a Circuit which measures AC Voltage and AC Current using MSP430F2619 and ADS131E08.
We have been able to interface with SPI very successfully and the bruises on ourforheads will heal soon.
We are able to measure MVDD correctly.
We are using a single Supply scheme. The Reference Voltage is 4V. OMPAMPOUT = 2.54V
We are interfacing this circuit with a Potential Transformer and have implemented the circuit shown on Pg. 49 Figure 51b.
Following are the values of the components:
R1 = 330K
R2 = 3.3K
R3 = 10K
RF= 470pF
The figure shows that there is no connection to the neutral. We have also left our neutral open. If we connect it to the AGnd, the transformer heats up. If we leave it open and measure the resultant voltage from the PT, then when the voltage is 8V AC the result is 0.015 Volts!
In the final installation the PT will have the ratio of 800/100, which should explain the selection of R1 and R2 values.
I am sure that the fault is in my understanding of the circuit. Could you please also guide me to some good resource along with your explanation.
Kind Regards,
Aditya
But when we connect the circuit to