Hello :
I am using a ADC12D1800 with the Xilinx K7 fpga. Now I am using 800M Hz sample rate, and the single is 70Mhz sine wave from singal generator. I test the ENOB is olny 6.9, and SNR is 42~44db. The test results did not perform a manual calibration. I read the TI technial document , that calibration can improve the ENOB. But how to perform a manual calibration. Is there more detailed description or a reference design.
I use the FPGA to pull up CAL pin for 3840 sample clocks after power up, But there is no effect , I doubt that I did not correctly calibrated the ADC12D1800.