Other Parts Discussed in Thread: ADC3421
How is differential input full-scale defined for the ADC3421?
Given these specifications:
Differential input full-scale voltage: 2 Vpp
Input common-mode voltage: 0.95 V
Then does this mean that the input pins INAP and INAM can be any voltage within the range of 0.45 V to 1.45 V, but nothing outside of this range?
.