I have two ADC12J4000EVM boards and would like to use an external 3.4Ghz clk and SYSREF to synchronize the two boards.
Both boards will use the 3.4Ghz as the sampling clock. The ADCs are configured in bypass mode with L8, F8, K4.
I would like to use the LMK04828 and was wondering if there is a recommended configuration for changing one or both of the boards?
Thanks,
John