Hallo,
I have a question about the ADS7865.
Is it always only 2 channels the channels can simultaneous sampling in the Sequencer Mode 1 or 2 of Figure 33 and Figure 34 in the datasheet?
The sampling is 3 times sampling of clock1 and clock21 and clock41 in Figure 34. And two channels can simultaneously sample each on Conv A and Conv B and Conv C conversion timings.
Best Regards,
Kazu Ogawa