This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error of WvBoardReadCaptureData: DUT Clock not detected by the firmware

The board works in NON-DESI mode. 2 signals are fed in both I+ and I- port on the board. I assume ADC works on 1.5Gsps and capture data on both of the 2 channels. The sample size is 16384. 

Right after WvBoardReadCaptureData is called, such error is returned. However, if DUT clock is not detected by firmware, the error ought be returned earlier. Please share me your thoughts. Thank you very much!

-Bridget 

15/02/04:23:58:10.0267:CAPTURE:Sending CMD_ID_CAPTURE_START with modifier:2

15/02/04:23:58:10.0270:GEN:DUT clock not detected by the firmware

15/02/04:23:58:10.0270:CMD:return:DLL_COMMAND_RET_ERROR_DUT_CLOCK_FREQ_INVALID

15/02/04:23:58:10.0270:CMD_API:Ack received.  Releasing API.

15/02/04:23:58:10.0270:CMD_API:==== Command complete     ====