Other Parts Discussed in Thread: ADS1248
I have a general, I think very easy question concerning ADS1248 analog frontend. I want to use the ADC on a Wheatstone Bridge.
The configuration should be as follow:
AVDD = 5V, DVDD = 3V, AVSS = 0V
Sensor Supply AVDD
Differential Measure
Voltage Reference Extern (Voltage Divider on AVDD): 2.5V
PGA 128
The datasheet says that the FS Input Range is +/-Vref/PGA, so in my case it is +/-19.53mV.
Assuming that I have a Signal Range from 0mV to 39mV, is it possible to shift the signal with the Offset Shift Register to -19.5V...19.5mV to use the complete ADC Input Range?
2nd question: is the Voltage Divider a possible, good solution to generate the external reference source?
Thanks for your help!