Other Parts Discussed in Thread: TVP7002
Hi, Dear Guys:
According to the datasheet, TVP7002's external clock ( pin name= "EXT_CLK", pin number="80") can be ADC sample clock ( instead of the H-PLL generated clock), and also can be as a timing reference for the mode detection block (instead of the internal clock reference) at a typical 27MHz frequency.
My questions are:
1) If I set it as the ADC sample clock, and the sampling frequency is 24.55MHz, it's working?
2) Instead of recommended 27MHz, while set for the sampling clock, can I still set it as the timing reference in 24.55MHz?
I didn't find the description of conflicting in the Control Register Definitions if set the above two.
Thank you.
Jason