This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Noise on pleth signal

Other Parts Discussed in Thread: AFE4490

I'm using the AFE9940 in push-pull mode with a reflective sensor.

The AFE9940 is programmed using the "example" settings as shown in the TI driver code.   The Pulse Repetition Frequency is set, as in the example, to 100 Hz.

I'm getting a signal, but there is a 20 Hz noise (sine wave) on top of the pleth waveform.

If I postprocess the datapoints, the 20 Hz peak (in the spectrum analysis) is clearly seen.    If I put the datapoints through a low-pass filter (again postprocessing in Matlab) to filter out the 20 Hz, the pleth waveform appears as expected.

The system actually has 3 AFE9940's in it.  They all exhibit the same 20 Hz noise.

The system is battery driven, so there is no connection to AC power.

I haven't been able to figure out what the source of the noise might be.

Can anyone suggest where the 20 Hz might be coming from?   Is there any possible source within the AFE9940.

Thanks!