Other Parts Discussed in Thread: ADS8688, ADS8684, TIDA-00307
I am testing the ADS8688 through SPI port of my MCU. Now I can see all the signals going into ADC are fine but nothing came out on SDO. One thing is my MCU is 3.3V VDD. Is this going to be a problem? Do I have to shift it to 5V. Is there a quick way to check the SPI on the ADC? Thanks, I think I got all the commands right, setting the ranges and manual channel select.
Any comments are greatly appreciated.
F.Z.