This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

"DSP not ready...retrying" ADS1282EVM-PDK Issue

Other Parts Discussed in Thread: ADCPRO, ADS1282

Hello,

I am trying to set up the ADS1282EVM-PDK and I am running into startup issues. After setting up the hardware and loading the ADS1282 plugin on ADCPro, I receive the following status messages: 

Reading Binary File > Downloading Binary File > USB connection established > Download Successful > DSP not ready... retrying > "The firmware load has failed due to a connection timeout..." > EVM/HW incompatible 

I am using Rev D of the MMB0 board with a Windows 7 PC. As directed here, I have the +/- 10V supplies connected to the J14 connector with the J13A jumper removed. I am also using an external 5V supply connected to the +5VA and GND terminals on J14 (with J12 disconnected). I noticed that although the driver installation process notifies that the NI-VISA and USBStyx drivers have been installed, they do not show up on Device Manager. Can I manually download and install all the drivers needed? I would appreciate any help. Thank you.