This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

connect two sets of TSW1400+TSW30SH84 to one PC

Hi there,

I am connecting two sets TSW1400+TSW30SH84 to one PC in order to generate 4 RF channels that are time aligned. Here is my problem.

 I connect to the first set of TSW1400+TSW30SH84, download firmware and waveform and setup is ok and I can see the transmission signal. Then from the GUI I disconnect to the first TSW1400 and connect to the second TSW1400. download firm is fine and I can see all LEDs are up. then I load waveform when click send button both TSW1400s LEDs are all off. The transmission signal is gone as well from the spectrum analyzer. What is problem here?

Thanks.