Other Parts Discussed in Thread: AFE4490, AFE4403, AFE4404EVM, AFE4404
We are using IC AFE4490 (QFN Package Industrial grade) for Heart Rate Measurement Application. We need clarification on the application circuit implementation.
Reference part: In AFE4403 (BGA Package) data sheet, it is mentioned that the TX3 pin driving the Green LED is used for heart rate measurement & the IR LED, Red LED is used for SP02 pulse oximetry application. (Ref: 8.3.5.1 Third LED Support, Page 39)
But in the AFE4490 part, there is no TX3 pin available. We are using the SFH7050 as sensor interface to AFE, which has IR, Red and Green LED then Photo detector.
Please clarify us, which pins from AFE are required to drive the SFH 7050 part & also specify which color LED is to be driven for the heart rate measurement application.
Regards,
S.Sathiya Seelan