Hi to all
I'm designing the new version of a 64 channels photodiode board using the new DDC232 ic.
1) There's a new pin called QGND, the datasheet says: "The QGND pin should be treated as a sensitive analog signal and connected directly to the supply ground with proper shielding." What does this means? Should I connect it to the same ground plane where I'll connect together AGND and DGND, or must it connected to the common kathodes of the 64 photodiodes array?
2) In the new application I would like to make interlaced integrations, where the first is 10 times shorter than the second (for instance 100us followed by 1ms), without losing integration time. I'm not sure if this is possible, since it's more likely a NON-CONTINUOUS mode, and in this mode only two short and equal integrations seems to be allowed, loosing integration time. I'hope this is "interlaced" mode can works, because I need to expand the dynamic range above the 20 bits. The idea is that If the integration made with 1ms saturate, than I'll use the integration made with 100us.
Thank you in advance,
Andrea