Other Parts Discussed in Thread: ADS1293
All,
We are using TIDA00096 as reference design. We have couple of questions regarding ecg channels and power consumption(using firmware in reference design):
1, if only one channel is used, how to connect ads1293? Let's say channel 1 is usded(PIN1 and 2), can I leave PIN3,4,5,6 floating? if not, how to treat other pins?
2.how much is the average power consumption of TIDA00096 when 3 channels are all running? We have tested a case with only one channel runing(other two channels floating), the current consumption is around 4-5mA on 4V supply. does this look right? it seems little bit high to me.
Appreciate any inputs.
-Kelv