Other Parts Discussed in Thread: MSP430F5529, DAC8728
Hi guys,
i have some problems with my DAC8728...i'm using it with the MSP430F5529 ...here the facts for the DAC:
AVDD = 15V; AVSS = -15V; DVDD = IOVDD = 3,3V; VREF = 5V
~USB/BTC is conected to GND ---> straight binary code
so when i set the device to default mode and try to convert some values i get some strage results:
input output
0x0 -15V
0x1000 -11.2V
0x2000 3.83V
0x3000 4.55V
0x8000 5.000V
0xA000 5.000V
0xB000 5.000V
0xC000 5.000V
i meassured the supplies--> they are ok also tried some other offset codes but the behavior is always strage like this...what could be the problem?
best regards stricker