Other Parts Discussed in Thread: AFE4400
hello i want to ask about my afe4400 , i want to connect chip afe4400 to my arduino board and this is my code on arduino board. i have connected my chip with this configuration
this is my arduino config
the configurations are
AFE_PDN --> ARD_PWDN
ADC_RESET --> ARD_START
ADC_RDY -- > ARD_DRDY
LED_ALM --> ARD_LED_ALM
SPI_MOSI --> ARD_MOSI
SPI_MISO --> ARD_MISO
SPI_SCK --> ARD_SCK
DIAG_END --> ARD_DIAG_END
SPI_CS0 --> ARD_CS0
PD_ALM --> ARD_PD_ALM
this is my code
#include <string.h>
#include <SPI.h>
#include <math.h>
//#include "Average.h"
#include <FIR.h>
#define CONTROL0 0x00
#define LED2STC 0x01
#define LED2ENDC 0x02
#define LED2LEDSTC 0x03
#define LED2LEDENDC 0x04
#define ALED2STC 0x05
#define ALED2ENDC 0x06
#define LED1STC 0x07
#define LED1ENDC 0x08
#define LED1LEDSTC 0x09
#define LED1LEDENDC 0x0a
#define ALED1STC 0x0b
#define ALED1ENDC 0x0c
#define LED2CONVST 0x0d
#define LED2CONVEND 0x0e
#define ALED2CONVST 0x0f
#define ALED2CONVEND 0x10
#define LED1CONVST 0x11
#define LED1CONVEND 0x12
#define ALED1CONVST 0x13
#define ALED1CONVEND 0x14
#define ADCRSTCNT0 0x15
#define ADCRSTENDCT0 0x16
#define ADCRSTCNT1 0x17
#define ADCRSTENDCT1 0x18
#define ADCRSTCNT2 0x19
#define ADCRSTENDCT2 0x1a
#define ADCRSTCNT3 0x1b
#define ADCRSTENDCT3 0x1c
#define PRPCOUNT 0x1d
#define CONTROL1 0x1e
#define SPARE1 0x1f
#define TIAGAIN 0x20
#define TIA_AMB_GAIN 0x21
#define LEDCNTRL 0x22
#define CONTROL2 0x23
#define SPARE2 0x24
#define SPARE3 0x25
#define SPARE4 0x26
#define SPARE4 0x26
#define RESERVED1 0x27
#define RESERVED2 0x28
#define ALARM 0x29
#define LED2VAL 0x2a
#define ALED2VAL 0x2b
#define LED1VAL 0x2c
#define ALED1VAL 0x2d
#define LED2ABSVAL 0x2e
#define LED1ABSVAL 0x2f
#define DIAG 0x30
#define BPM_WINDOW 300
#define count 60
int IRheartsignal[count];
int Redheartsignal[count];
int IRdc[count];
int Reddc[count];
double difIRheartsig_dc;
double difREDheartsig_dc;
double powdifIR;
double powdifRed;
double IRac;
double Redac;
double SpOpercentage;
double Ratio;
const int SOMI = 12;
const int SIMO = 11;
const int SCLK = 13;
const int SPISTE = 7;
const int SPIDRDY = 6;
int pin = 3;
int pin2 = 4;
volatile int state = LOW;
void AFE4490Init (void);
void AFE4490Write (uint8_t address, uint32_t data);
uint32_t AFE4490Read (uint8_t address);
signed long average_BPM( signed long );
//--------------------------------------------------------------------------------------------------------------------
#define CES_CMDIF_PKT_START_1 0x0A
#define CES_CMDIF_PKT_START_2 0xFA
#define CES_CMDIF_TYPE_DATA 0x02
#define CES_CMDIF_PKT_STOP 0x0B
volatile char DataPacketHeader[5];
volatile char DataPacketFooter[2];
volatile int datalen = 135;
unsigned long time;
volatile byte SPI_RX_Buff[150] ;
volatile static int SPI_RX_Buff_Count = 0;
volatile char *SPI_RX_Buff_Ptr;
volatile int Responsebyte = false;
volatile unsigned int pckt =0 , buff=0,t=0 , j1=0,j2=0;
volatile unsigned long int EEG_Ch1_Data[150],EEG_Ch2_Data[150];
volatile unsigned char datac[150];
unsigned long ueegtemp = 0, ueegtemp2 = 0, Pkt_Counter=0;
signed long seegtemp=0, seegtemp2=0;
volatile int i;
FIR fir;
void setup()
{
Serial.begin(57600);
SPI.begin();
pinMode (SOMI,INPUT);
pinMode (SPISTE,OUTPUT);
pinMode (SCLK, OUTPUT);
pinMode (SIMO, OUTPUT);
pinMode (SPIDRDY,INPUT);
pinMode(2, INPUT);
pinMode(3, OUTPUT);
//pinMode(pin, OUTPUT);
attachInterrupt(0, blink, RISING );
SPI.setClockDivider (SPI_CLOCK_DIV8);
SPI.setDataMode (SPI_MODE0);
SPI.setBitOrder (MSBFIRST);
//-------------------------------------------
DataPacketHeader[0] = CES_CMDIF_PKT_START_1;
DataPacketHeader[1] = CES_CMDIF_PKT_START_2;
DataPacketHeader[2] = (datalen);
DataPacketHeader[3] = (datalen >> 8);
DataPacketHeader[4] = CES_CMDIF_TYPE_DATA;
DataPacketFooter[0] = 0x00;
DataPacketFooter[1] = CES_CMDIF_PKT_STOP;
//-------------------------------------------------
float coef[FILTERTAPS] = { 0.021, 0.096, 0.146, 0.096, 0.021};
fir.setCoefficients(coef);
//declare gain coefficient to scale the output back to normal
float gain = 1; // set to 1 and input unity to see what this needs to be
fir.setGain(gain);
AFE4490Init ();
}
/////////////////////////////////////////////////////////////////////////////////////////////////////////////////
void loop()
{ // for(int i = 0; i<count; i++)
//if (0)
// Serial.println("TEST3");
if (state == HIGH)
{
//noInterrupts();
detachInterrupt(0);
digitalWrite(3, 1); //test pin 3
digitalWrite(3, 0);
// Serial.println("TEST3");
//delay(10);
AFE4490Write(CONTROL0,0x000001);
ueegtemp = AFE4490Read(LED1VAL);
ueegtemp =ueegtemp;
//ueegtemp2 = AFE4490Read(LED1VAL);
Responsebyte = true;
/* AFE4490Read(LED1VAL);
AFE4490Read(LED2VAL);
*//*Serial.print(AFE4490Read(LED1VAL));
Serial.print("\t");
Serial.println(AFE4490Read(LED2VAL));
*/
}
if(Responsebyte == true)
{
//for(t=0; t< 1 ; t++)
{
buff = 0;
Pkt_Counter++; //if(Pkt_Counter > 0) Pkt_Counter = 0x00;
datac[buff++] = 0xA0; // sync0
datac[buff++] = 36; //sync1
datac[buff++] = (unsigned char)(Pkt_Counter >> 24);
datac[buff++] = (unsigned char)(Pkt_Counter >> 16);
datac[buff++] = (unsigned char)(Pkt_Counter >> 8);
datac[buff++] = (unsigned char)(Pkt_Counter );
ueegtemp = (unsigned long) (ueegtemp<<10);
seegtemp = (signed long) (ueegtemp);
seegtemp = (signed long) (seegtemp>>10);
// Serial.println(seegtemp);
// Serial.println("TEST2");
// seegtemp = seegtemp - average_BPM(seegtemp);
seegtemp = seegtemp*100;
// seegtemp = fir.process(seegtemp);
//Serial.println(seegtemp);
ueegtemp2 = (unsigned long) (ueegtemp2<<10);
seegtemp2 = (signed long) (ueegtemp2);
seegtemp2 = (signed long) (seegtemp2>>10);
/*for(i=3000;i<seegtemp;i+=10)
{
Serial.print("*");
//Serial.print("hai");
}
Serial.println(" ");
*/
pckt+= 3;
//seegtemp = seegtemp*5
datac[buff++] = (unsigned char) (seegtemp);
datac[buff++] = (unsigned char) (seegtemp>>8); //>>8
datac[buff++] = ( unsigned char) (seegtemp >> 16); //>>16
datac[buff++] = (unsigned char) (seegtemp >>24);
//Serial.println(seegtemp);
/*datac[buff++] = (unsigned char) (seegtemp2);
datac[buff++] = (unsigned char) (seegtemp2>>8); //>>8
datac[buff++] = ( unsigned char) (seegtemp2 >> 16); //>>16
datac[buff++] = (unsigned char) (seegtemp2 >>24);
*/
for(i=0;i<28;i++) // fill channel 1 buff
{
//ueegtemp = (uint16_t) ( (EEG_Ch1_Data[pckt+1]<<8)| EEG_Ch1_Data[pckt]);
//seegtemp = (int16_t) (ueegtemp);
//pckt++
//datac[buff++] = EEG_Ch1_Data[pckt++] ;
datac[buff++] = 0x00 ;
}
datac[buff++] = 0xc0;//(uint8_t)seegtemp ;
//Serial.println(seegtemp);
for(i=0; i<39; i++) // transmit the data
{
Serial.write(datac[i]);
//udi_cdc_putc(datac[i]);
//cpu_delay_us(90, 48000000);
}
// cpu_delay_us(100, 48000000);
}
//SPI_RX_Buff_Count = 0;
Responsebyte = false;
state = LOW;
attachInterrupt(0, blink, RISING );
/*
Serial.print("Stop Time: ");
time = millis();
//prints time since program started
Serial.println(time);
*/
}
}
signed long average_BPM( signed long bpm)
{
static int bpm_sample_count;
static signed long bpm_store[BPM_WINDOW];
signed long bpm_sum =0, bpm_avg=0;
if (bpm_sample_count < BPM_WINDOW)
bpm_store[bpm_sample_count++] = bpm;
else
{
for(i=0 ; i<BPM_WINDOW-1 ; i++)
bpm_store[i] = bpm_store[i+1] ;
bpm_store[BPM_WINDOW-1] = bpm;
}
/*
Serial.println("\nbpm_store\t");
for(i=0 ; i<BPM_WINDOW ; i++)
{
Serial.print(bpm_store[i]);
Serial.print("\t");
}
Serial.print("\nbpm_sample_count\t");
Serial.println(bpm_sample_count);
*/
for(i=0 ; i<BPM_WINDOW ; i++)
bpm_sum += bpm_store[i];
/*
Serial.print("\nbpm_sum\t");
Serial.println(bpm_sum);
*/
bpm_avg = bpm_sum/(bpm_sample_count);
/*
Serial.print("\nbpm_avg\t");
Serial.println(bpm_avg);
*/
return (bpm_avg);
}
void blink()
{
state = HIGH;
}
/////////////////////////////////////////////////////////////////////////////////////////////////////////////////
void AFE4490Init (void)
{
Serial.println("AFE4490 Initialization Starts");
AFE4490Write(CONTROL0,0x000000);
AFE4490Write(TIAGAIN,0x000000); // CF = 5pF, RF = 500kR
AFE4490Write(TIA_AMB_GAIN,0x000005); // Timers ON, average 3 samples
AFE4490Write(LEDCNTRL,0x0011414);
AFE4490Write(CONTROL2,0x000000); // LED_RANGE=100mA, LED=50mA
AFE4490Write(CONTROL1,0x010707); // Timers ON, average 3 samples
AFE4490Write(PRPCOUNT, 0X001F3F);
/*AFE4490Write(CONTROL1, 0x000101);
AFE4490Write(CONTROL2, 0x000000);
AFE4490Write(PRPCOUNT, 0X001F3F);*/
AFE4490Write(LED2STC, 0X001770); //timer control
AFE4490Write(LED2ENDC,0X001F3E); //timer control
AFE4490Write(LED2LEDSTC,0X001770); //timer control
AFE4490Write(LED2LEDENDC,0X001F3F); //timer control
AFE4490Write(ALED2STC, 0X000000); //timer control
AFE4490Write(ALED2ENDC, 0X0007CE); //timer control
AFE4490Write(LED2CONVST,0X000002); //timer control
AFE4490Write(LED2CONVEND, 0X0007CF); //timer control
AFE4490Write(ALED2CONVST, 0X0007D2); //timer control
AFE4490Write(ALED2CONVEND,0X000F9F); //timer control
AFE4490Write(LED1STC, 0X0007D0); //timer control
AFE4490Write(LED1ENDC, 0X000F9E); //timer control
AFE4490Write(LED1LEDSTC, 0X0007D0); //timer control
AFE4490Write(LED1LEDENDC, 0X000F9F); //timer control
AFE4490Write(ALED1STC, 0X000FA0); //timer control
AFE4490Write(ALED1ENDC, 0X00176E); //timer control
AFE4490Write(LED1CONVST, 0X000FA2); //timer control
AFE4490Write(LED1CONVEND, 0X00176F); //timer control
AFE4490Write(ALED1CONVST, 0X001772); //timer control
AFE4490Write(ALED1CONVEND, 0X001F3F); //timer control
AFE4490Write(ADCRSTCNT0, 0X000000); //timer control
AFE4490Write(ADCRSTENDCT0,0X000000); //timer control
AFE4490Write(ADCRSTCNT1, 0X0007D0); //timer control
AFE4490Write(ADCRSTENDCT1, 0X0007D0); //timer control
AFE4490Write(ADCRSTCNT2, 0X000FA0); //timer control
AFE4490Write(ADCRSTENDCT2, 0X000FA0); //timer control
AFE4490Write(ADCRSTCNT3, 0X001770); //timer control
AFE4490Write(ADCRSTENDCT3, 0X001770);
delay(1000);
Serial.println("AFE4490 Initialization Done");
}
/////////////////////////////////////////////////////////////////////////////////////////////////////////////////
void AFE4490Write (uint8_t address, uint32_t data)
{
digitalWrite (SPISTE, LOW); // enable device
SPI.transfer (address); // send address to device
SPI.transfer ((data >> 16) & 0xFF); // write top 8 bits
SPI.transfer ((data >> 8) & 0xFF); // write middle 8 bits
SPI.transfer (data & 0xFF); // write bottom 8 bits
digitalWrite (SPISTE, HIGH); // disable device
}
/////////////////////////////////////////////////////////////////////////////////////////////////////////////////
uint32_t AFE4490Read (uint8_t address)
{
uint32_t data=0;
digitalWrite (SPISTE, LOW); // enable device
SPI.transfer (address); // send address to device
//SPI.transfer (data);
data |= (SPI.transfer (0)<<16); // read top 8 bits data
data |= (SPI.transfer (0)<<8); // read middle 8 bits data
data |= SPI.transfer (0); // read bottom 8 bits data
digitalWrite (SPISTE, HIGH); // disable device
/* pinMode (SOMI,OUTPUT);
digitalWrite (SOMI, HIGH);
delay(1);
pinMode (SOMI,INPUT);
*/
return data; // return with 24 bits of read data
}
i have several problem which are :
1. last time, i have trouble in connecting this small chip into my printed pcb board. at first i try to arrange it so the pin is matched with the routing manually. but suddenly this chip is getting hot. So finally i have soldered that chip but it dontgive any result.
i have checked it the sign of life of afe4400 chip. but it has different result with what stated in FAQ section
1. tx-ref_pin = 0.11 V
2. BG = 0.65 V
3. VCM = 1.12 V
voltage tx_ref/led_drv and rx_ana/rx_div, both are supplied from arduino uno board which value is 3.3 V
i am suspicious that i have damage my chip, is there any way to test that my chip can still work?
2. is there any proper way to make the chip connected to printed board without damaging it? any soldering reccomendation?
3. is there any other references code that can help my case? right now i am designing a photoplethysmograph sensor based on afe4400 chip
4. is my configuration is right? i use 22pF instead 18pF as stated in datasheet, i also supply LED_DRV_SUP, TX_CTRL_SUP, RX_DIG_SUP, RX_ANA_SUP with 3.3 V because, 3.3 V is only available supply in my system.
5. i have connected led and IR like in the datasheet, i have tried both configuration, common anode and H-bridge, but it still dont give any result. i have tested pin INP , INM, TXM and TXP
pin INP : 0.07V
pin INM : 0.02V
pin TXM : 0.35V
pin TXP : 0.35 V
with my above code, the result of register led1val is always 0.
i have check it with giving a led in ADC_RDY pin to tell me when the ADC_RDY is updated and reset, but the result is still none.
FYI, i bought raw chip, not evaluation module
thanks, pardon for my mistake because english is not my native
i look forward to your help
regards.