Other Parts Discussed in Thread: ADC08D1520, LP38513-ADJ
The operation and according observation are described as following
1. power up ADC board;
2. start wavevision 5 on windows 7
3. connect usb with reference board and PC.
4. we observe wavevision search hardware and load fpga image
5. 3 LEDs, fpga_operational, and ecem_enabled, and rcout1/2/enabled, are on. However, ADC_POWER is not on.
6. VM16ABE3 turns to high temperature easily. The power on VM16ABE3 's 1st pin is 5V and 4th pin is 0.5V.
What is the reason? Why the ADC_POWER cannot be powered up?
Thanks.
-Bridget