Hi, I am using VSP3210 with Hamamatsu CCD sensor (S8982) . The circuit does not work properly. The circuit assembled on 4 layer PCB with separate DGND and AGND (in one layer) joined at one point under ADC and separated by cutouts,similarly for digital and analog power supply. Analog supply obtained from digital and isolated from digital.
ADCCK 1 Mhz
CK1 rise 300ns after ADCCK rise, fall 100ns before ADCCK fall
CK2 rise 300 ns after ADCCK fall, fall 100ns before ADCCK rise
ADC used in 1-CCD mode; for signal from CCD used Red channel. Config Reg = 0x88; Red Bias = 0x200;Red Gain = 0x00;
/OE = GND allways; CLP = VCC during unused black pixels; VDRV = +3.3V;
Problem is the next: When I don't connect CCD to my board, and Input signal coupled from DC by 0.1 uF. R = 5.1 kOh input resistor for emitter follower for CCD. I see several spikes on my picture (all pixel is a noise near 12 rms). Spikes have constant amplitude max - min codes from ADC (0x4FF(1279) - 0x200 (512)= 0x2FF (767) ) and consist from two pixel with min code and next with max code. If I change gain to 5 from 0 or change only bias to 0x1FD I see much more spikes on my picture.
I think it may be wrong ADC convert. What do you suggest me for correct this problem?