This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131E08EVM-PDK software continuous mode question.

Other Parts Discussed in Thread: ADS131E08EVM-PDK, ADS131E08, ADCPRO

Hello,

I am using the ADS131E08EVM-PDK and wish to continuously log samples to file. Is there any way to do this?

I am using the ADS131E08 Evaluation Software version 1.0.0.2.

Continuous mode doesn't appear to update any files. Save to File only saves the last sample set.

I have seen similar requests pointed to ADCPro. Is ADCPro compatible with the ADS131E08EVM-PDK?

Thanks!

  • Hello Christopher -
    The software only has the ability to log data once the acquisition is completed (ie after the Single Acquistion). Since the 'Contiuous' mode is just a repeated 'Single Acquisition', we did not include the save data since there can be samples missing between the acquire loops.
  • Do you think this will ever be implemented?

    Is there any way to get that continuous log? 

    Is there any way to get a continuous log with gaps?

  • Hello Christopher -
    We do not have plans to implement continuous logging features in the software.
    Currently, you can only save one acquisition period at a time and then save it.

    We can offer the source files (LabView and DSP) so you can build upon what we have done for your own design purposes. However, these files are provided as-is and we cannot supported changes to the application or firmware.