Other Parts Discussed in Thread: ADS1230, ADS1232
please help to share ADS1230 sample code interfaced with TI mcu as well as if with any other mcu.
Also please share ADS1230evm sample code.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sheetal,
All design files/firmware/software for the ADS1230REF can be found on the TI public ftp server:
ftp://ftp.ti.com/pub/data_acquisition/ADS123xREF/ADS123x_CDROM/
Best regards,
Bob B
Sir,
Thanks for sharing details, But in this link the source code is for ADS1232.
Need source code for ADS1230.
Please share same.
Hi Sheetal,
The firmware for the ADS1230 and ADS1232 is the same other than the data length of the SPI capture and the channel count/temp sensor which is determined by compiler directive. The only difference between the devices is the ADS1230 is 20-bit while the ADS1232 is 24-bit, has two channels and a temp sensor.
Best regards,
Bob B