Hi,
We are developing HRM based on AFE4400 on Android. We are trying to validate it on AFE44x0SPO2EVM board. We have set the PRF to 400Hz with a duty cycle of 25%.
We are observing that after software reset, the read to these registers returns 0, which is as expected. But after configuring the control and timing registers, we are always getting ADC_RDY interrupt on the host processor side. Further testing revealed that the LED and Ambient LED digital sample value registers are getting updated even when the PULSEOx Cable is not connected to the DB9-F connector.
We are confused as to how the LED and ALED digital sample registers are getting updated without connecting the finger sensor pulse oximeter cable.
Could you please advise us on this?
Thank You.