HI i have a problem can't solve it .
i'm working in project with ADS1210P but i can't found any software where can be simulated
even a packages in TINA-TI
PLZ help me i'm helpless
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jbali,
Welcome to the forum! Do you actually have an ADS1210P? You may have a hard time getting one if you don't already have one. I'm going to make a guess that you chose this part because of the DIP package which is easier to prototype.
To answer your question it is next to impossible to create a simulation that would encompass this part or most delta-sigma data converters. There are too many variations of operation that interact with each other. You could build your own analog input simulation based on Figure 11 of the datasheet. The digital filter is sinc3 and info is on page 12 of the datasheet.
If I knew a little more about your application I might be able to suggest an easier part to work with than the ADS1210 which is quite an old part. Is there something specific you would like to determine from simulation?
Best regards,
Bob B
Hi Jbali,
The ADS1210P is not recommended for new design as the DIP package is reaching obsolescence. For weigh scale designs with integrated amplifiers take a look at the following devices:
ADS1220
ADS1230
ADS1231
ADS1232
Best regards,
Bob B