This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC128S102 input and power conditioning



Hello,

I'm using the ADC128S102QML and have questions about conditioning the inputs as well as possible work-arounds for some of its vulnerabilities.

My first question is about input conditioning.  Although a low source impedance is recommended, we have a high source impedance and would like to keep it that way (for isolation and to eliminate extra parts).  One solution we've considered is idling the clock to the ADC during the tracking phase so that tracking happens for a longer time.  Similarly, we've considered giving the device an extra falling edge of the clock so that it enters tracking mode for the long period between samples (we sample at a rate of 800 us).  It seems like the device would tolerate a long tracking period (clock stuck low at clock 1), but can someone at TI verify that this is OK?  Some of our ideas depend on what happens to the internal sampling cap, whether it gets depleted after each sample, whether it gets charged somewhere, or whether it retains the previous sample.  Can someone explain what happens to the charge on the cap after a conversion please?

Another question we have is about the input protection.  We do have some inputs that are driven by op-amps, but those op-amps are powered by rails (+/-5V) that exceed the ADC (4V).  During turn on and off (or due to a failure), it's possible the input to the ADC could step out of the absolute maximum ratings.  Can the protection diodes handle some current for these times?  We assume we can put 1k in series with them (again, raising the source impedance) to limit the current to +/-5 mA below maximum limit, is that safe enough?  Do we need external diodes?

Finally, regarding the power sequence requirement that Va be at or above Vd, we will likely violate this unless we change our supplies.  Can we get away with using an external Schottky diode from Vd to Va so that the internal one doesn't get turned on?  Looks like the spec sheet says the ADC can tolerate 300 mV.  We're talking about a short period, hundreds of ms at most.

Thanks for the help,

Robert

  • first question: your ideas for extending the track time are valid and the part will behave well in the fashion you have suggested. the sample cap will just discharge through parasitic path, it does not get discharged or charged unless you are in track mode and it is connected to the input pin

    you need to limit the current with source resistors or some other means if the inputs are going above the supply voltage VA; depending on the number of inputs that are subject to the elevated input voltage, you may need to limit the current on each pin to different values; each pin has a max rating of 10mA but the total current for all the pins is not to exceed 20mA; using a series resistor of 1k as you suggested would limit the input current on any pin to less than 5mA assuming an input of 5V above or below VA and no other protection would be required

    your suggestion of Schottky diode is valid and would prevent internal diode from conducting the current

    with all of this said, it is not possible for me to determine any long term negative impact of sourcing or sinking elevated currents into the inputs. all of your suggested workarounds are valid but operating near absolute max specs is not generally recommended

    feel free to contact me directly at chuck.sins@ti.com if you have any further questions
    thanks, Chuck
  • Thanks!  We don't expect to get out of range except for possibly power cycling, or a failure.