ADS8684
Please tell us about the treatment of unused pins.
1) NC-pin (12,13,14,15) Do you need to Floating state? or do I connect to GND?
2) When you do not use the AUX_IN pin (10), or you need to Floating state?
3) When you do not use the AIN_xP pin (18,21,23), or you need to Floating state? or do I connect to GND?
4) When you do not use the AIN_xP pin (18,21,23) between AIN_xGNA (19,20,22) pin do i need to connect a capacitor (for example 1uF).
Best regards