This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

source code for the AVM GUI running on PC:

Other Parts Discussed in Thread: MSP430F5529, ADS1292

I want to change the pin assignments in the MSP430f5529 to siute te MSP430f5529 Launch pad board so that the custom board that I have assemle works wih the launch pad.- would this only do the job or something needs to be done on the GFUI source code as well.

Can you give me the flow diagram of the EVM:

power on->xxxxx->xxxxx-> LOAD THE FIRMWARE IN THE mcp430f5529 ->XXXX->XXXX

Is this what is typically done by the board. 

If yes 

where is the firmware klocated? or does the CCS compiles the firmwhere from a perticulaer address - what is that address

could you help me on this so that i can  odify the pin assignments and make a "booster pack for my own use" this of course would mean that the pin assignments would need to be changed totally PLEASE HELP URGENTLY

Regards

Viney Chaddha.